This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6457硬件连接DDR2问题

借用TI例子,利用CSL函数编写DDR2接口驱动,正常初始化完成,外片DDR2寻址读写数据正常。以为DDR2驱动没有,后来有一块板子,DDR2芯片供电异常,原来1.8V供电,这个板子0.9V。可是C6457跑仿真,DDR2驱动初始化正常,同样片外DDR2寻址读写数据正常。。。。。。。。找半天也搞不清楚如何进行片外硬件连接是否正常的状态检测。请教下,这种现象,我驱动编写是否正常?DDR2芯片如何检测硬件是否正常?

  • 0.9v是不是量的是VREFSSTL参考电压(0.5 × DVDD18)?
  • 是DDR2芯片的供电电压,,参考电压也是0.9V。后面把DDR2供电电压调整为1.8V,参考电压还是0.9V。

    我的疑惑是,,外设DDR2不正常,驱动片外寻址读写正常,,,,,,我怎么判断DDR2有没有接好??
  • 或者是 我读写的数据全在DDR2接口缓冲区里,其实并没有写到外设DDR2??
  • 或者说 我DDR2驱动读写测试,数据全在片内缓冲区里,并没有真正写到片外??

    驱动配置方式:
    1、status = CSL_ddr2Init(NULL)
    2、hDdr2 = CSL_ddr2Open(&ddr2Obj, CSL_DDR2, NULL, &status)
    3、status =CSL_ddr2HwSetup(hDdr2, &hwSetup)

    参数部分省略,DDR2读写地址为0xE0000000开始

    无论片外DDR2芯片供电是否异常,驱动配置方式 status 均为OK, DDR2读写数据对比正常。

    DDR2芯片连接是否正常通过什么来判断??还有就是如何确定数据是否已经写到片外DDR2或者从DDR2读取到数据?