This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354问题

Other Parts Discussed in Thread: AM3354

我们在3354上出现了两个比较奇怪的问题。麻烦帮忙看看能不能解决。谢谢~~

   1、线程不能被调度:  现在在我们AM3354上跑的linux系统,里面打了个实时Xenomai 补丁,系统有一个xenomai线程和linux下的一个线程,

但是在跑的过程中有一定概率(小概率,有可能一两天出现一次)会出现linux下的线程不能被调度的问题(这个进程有时候10几秒钟到几十秒都没有被调度),延时了很久,后面又恢复了。

   2、串口发送数据窜位:通过3354的串口做了485总线。系统每次上电会与下位机握手发送 0x01、0X50、0x00、0x1C,这四个数放入串口发送buffer,但是

有时在上电的时候有可能与下位机握手不上,这时候从3354的TX管脚上测得数据为0x1c、0x01、0x50、0x00.出现了数据窜位。