我目前使用6670LE EVM板调试一个以太程序,用的是packages带的PA_EmacExample例子,但用的时候碰到了几个问题,第一是如果想使用外环模式的话,在有一个SGM等BIT位的地方过不去,不过参考《C6678千兆网调试及性能问题》这个帖子,知道6670的板子PORT0接到了AMC总线上,所以需要修改为PORT1,我按照 Marvin Liang的回复替换了cpsw_mgmt.c文件,不过还是依然等不过去,仔细检查了serdes的配置,发现这样的疑问,就是对tx寄存器的配置,代码中是CSL_BootCfgSetSGMIITxConfig (1, 0x000108A1),但仔细查阅手册,其中第4,5位手册推荐01,其他不认可,而代码是10,不知道有什么考虑,我修改为CSL_BootCfgSetSGMIITxConfig (1, 0x11F91),能等过去了,只是send却只能达到50包左右就获取不到free的队列了(长度1024),不知道什么原因,请帮忙解答一下!