This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

kernel启动优化



大家好,我正在做AM335x的启动时间优化,目前uboot版本为2016.05,linux kernel版本为4.1.8。由于使用nand flash,读写速度超慢,移植论坛上优化nand读写速度的patch后,读写速度确实提升一半。现在又遇到一个问题,在uboot引导完kernel后,打印最后一条log信息starting kernel...后,就启动kernel了,然后kernel开始初始化,自解压,到kernel启动后打印的第一条log时,耗时为2.27s,太不可思议,这个过程怎么会耗时这么久。前段时间做imx6的,这个过程才700ms,这个差距太大了,请教IT的各位技术高手,帮忙指导下,感激不尽