各位大牛:本人刚接触6670不久 在跑pa_emac的例程时,用evm板能跑通,但用在仿真下部能通过,会报
TMS320C66x_0: Warning: Source MAC address & MAC address specified in config file don't match.
这样的警告,并且程序运行时事一直收不到包的
[TMS320C66x_0] **************************************************
[TMS320C66x_0] ******* Ethernet Single Core Example Start *******
[TMS320C66x_0] **************************************************
[TMS320C66x_0] QMSS successfully initialized
[TMS320C66x_0] CPPI successfully initialized
[TMS320C66x_0] PASS successfully initialized
[TMS320C66x_0] Ethernet subsystem successfully initialized
[TMS320C66x_0] Tx setup successfully done
[TMS320C66x_0] Rx setup successfully done
[TMS320C66x_0] PASS setup successfully done
[TMS320C66x_0] Packet Transmission Start ...
[TMS320C66x_0] Packet Transmission Done.
[TMS320C66x_0] Wait for all packets to be Received ...
[TMS320C66x_0] Received 0 packets so far...
[TMS320C66x_0] Received 0 packets so far...
[TMS320C66x_0] Received 0 packets so far...
[TMS320C66x_0] Received 0 packets so far...
不知道在仿真器的设置中需要修改什么和在程序中需要修改什么,请大神指点