This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

iwr1642 关于ppcount 开发者模式

Other Parts Discussed in Thread: IWR1642, SYSBIOS

当我进行编译并把.bin文件烧入iwr1642后,

在debug模式却无法正常运行雷达,并且会出现如下错误

[C674X_0] Debug: Logging UART Instance @00815e30 has been opened successfully
Debug: DSS Mailbox Handle @0080d8c8
Debug: MMWDemoDSS create event handle succeeded
Debug: MMWDemoDSS mmWave Control Initialization succeeded
Debug: MMWDemoDSS ADCBUF Instance(0) @00815e18 has been opened successfully
Debug: MMWDemoDSS Data Path init succeeded
Debug: MMWDemoDSS initTask exit
[Cortex_R4_0] Debug: Heap before creating a tracker
Debug: System Heap (TCM): Size: 65536, Used = 27864, Free = 37672 bytes
Exception occurred in ThreadType_Task.
Task handle: 0x8005c08.
Task stack base: 0x8005c58.
Task stack size: 0x1000.
R0 = 0x3d4ccccd R8 = 0x00000000
R1 = 0xc2c80000 R9 = 0x00000000
R2 = 0x42c80000 R10 = 0x000041f0
R3 = 0x00000000 R11 = 0xffffffff
R4 = 0x08008a00 R12 = 0x00000001
R5 = 0x08006a1c SP(R13) = 0x08006820
R6 = 0x42c80000 LR(R14) = 0x00013118
R7 = 0x08008a70 PC(R15) = 0x0000620e
PSR = 0x200c019f
DFSR = 0x00000001 IFSR = 0x00000000
DFAR = 0x3d4ccccd IFAR = 0x00000000
ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x0000620e, lr = 0x00013118.
xdc.runtime.Error.raise: terminating execution