This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCASP自环不成功。



我项目上用OMAPL138的板子MCASP的引脚都是链接的FPGA,所以在FPGA这端设置的MCASP自环。把axr0接收到的通过axr1发回去。

部分代码如下

input mcasp_afsx,
input mcasp_ahclkx,
input mcasp_aclkx,
input axr0,

output mcasp_afsr,
output mcasp_ahclkr,
output mcasp_aclkr,
output axr1,

assign mcasp_afsr = mcasp_afsx;
assign mcasp_aclkr = mcasp_aclkx;
assign mcasp_ahclkr = mcasp_ahclkx;
assign axr1 = axr0;

在OMAPL138这端,通过axr0接口发固定的数,axr1接收。

在配置MACASP的时候,发送全部取内部时钟,接收全部取外部时钟。

一直循环发送,但是接收不到。在FPGA端也没有看到时钟和信号的波形。

部分代码如下,关于edma3的部分未做变化。

static void McASPI2SConfigure(void)
{
McASPRxReset(SOC_MCASP_0_CTRL_REGS);
McASPTxReset(SOC_MCASP_0_CTRL_REGS);

/* Enable the FIFOs for DMA transfer */
McASPReadFifoEnable(SOC_MCASP_0_FIFO_REGS, 1, 1);
McASPWriteFifoEnable(SOC_MCASP_0_FIFO_REGS, 1, 1);

/* Set I2S format in the transmitter/receiver format units */
McASPRxFmtI2SSet(SOC_MCASP_0_CTRL_REGS, WORD_SIZE, SLOT_SIZE,
MCASP_RX_MODE_DMA);
McASPTxFmtI2SSet(SOC_MCASP_0_CTRL_REGS, WORD_SIZE, SLOT_SIZE,
MCASP_TX_MODE_DMA);

/* Configure the frame sync. I2S shall work in TDM format with 2 slots */
McASPRxFrameSyncCfg(SOC_MCASP_0_CTRL_REGS, 2, MCASP_RX_FS_WIDTH_WORD,
MCASP_RX_FS_EXT_BEGIN_ON_FALL_EDGE);
McASPTxFrameSyncCfg(SOC_MCASP_0_CTRL_REGS, 2, MCASP_TX_FS_WIDTH_WORD,
MCASP_TX_FS_INT_BEGIN_ON_RIS_EDGE);

/* configure the clock for receiver */
McASPRxClkCfg(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_EXTERNAL, 0, 0);
McASPRxClkPolaritySet(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_POL_RIS_EDGE);
McASPRxClkCheckConfig(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLKCHCK_DIV32,
0x00, 0xFF);

/* configure the clock for transmitter */
McASPTxClkCfg(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_INTERNAL, 11, 1);
McASPTxClkPolaritySet(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_POL_FALL_EDGE);
McASPTxClkCheckConfig(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLKCHCK_DIV32,
0x00, 0xFF);

/* Enable synchronization of RX and TX sections */
McASPTxRxClkSyncEnable(SOC_MCASP_0_CTRL_REGS);

/* Enable the transmitter/receiver slots. I2S uses 2 slots */
McASPRxTimeSlotSet(SOC_MCASP_0_CTRL_REGS, I2S_SLOTS);
McASPTxTimeSlotSet(SOC_MCASP_0_CTRL_REGS, I2S_SLOTS);

/*
** Set the serializers, Currently only one serializer is set as
** transmitter and one serializer as receiver.
*/
McASPSerializerRxSet(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_RX);
McASPSerializerTxSet(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX);

/*
** Configure the McASP pins
** Input - Frame Sync, Clock and Serializer Rx
** Output - Serializer Tx is connected to the input of the codec
*/
McASPPinMcASPSet(SOC_MCASP_0_CTRL_REGS, 0xFFFFFFFF);
McASPPinDirOutputSet(SOC_MCASP_0_CTRL_REGS,MCASP_PIN_AXR(MCASP_XSER_TX));
McASPPinDirInputSet(SOC_MCASP_0_CTRL_REGS, MCASP_PIN_AFSX
| MCASP_PIN_ACLKX
| MCASP_PIN_AHCLKX
| MCASP_PIN_AXR(MCASP_XSER_RX));

/* Enable error interrupts for McASP */
McASPTxIntEnable(SOC_MCASP_0_CTRL_REGS, MCASP_TX_DMAERROR
| MCASP_TX_CLKFAIL
| MCASP_TX_SYNCERROR
| MCASP_TX_UNDERRUN);

McASPRxIntEnable(SOC_MCASP_0_CTRL_REGS, MCASP_RX_DMAERROR
| MCASP_RX_CLKFAIL
| MCASP_RX_SYNCERROR
| MCASP_RX_OVERRUN);
}

static void I2SDataTxRxActivate(void)
{
/* Start the clocks */
McASPRxClkStart(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_EXTERNAL);
McASPTxClkStart(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_INTERNAL);

/* Enable EDMA for the transfer */
EDMA3EnableTransfer(SOC_EDMA30CC_0_REGS, EDMA3_CHA_MCASP0_RX,
EDMA3_TRIG_MODE_EVENT);
EDMA3EnableTransfer(SOC_EDMA30CC_0_REGS,
EDMA3_CHA_MCASP0_TX, EDMA3_TRIG_MODE_EVENT);

/* Activate the serializers */
McASPRxSerActivate(SOC_MCASP_0_CTRL_REGS);
McASPTxSerActivate(SOC_MCASP_0_CTRL_REGS);

/* make sure that the XDATA bit is cleared to zero */
while(McASPTxStatusGet(SOC_MCASP_0_CTRL_REGS) & MCASP_TX_STAT_DATAREADY);

/* Activate the state machines */
McASPRxEnable(SOC_MCASP_0_CTRL_REGS);
McASPTxEnable(SOC_MCASP_0_CTRL_REGS);
}

请问:问题出在哪了,时钟按照这样配是否有错。