This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ERROR: Cache unsupported on device!

Other Parts Discussed in Thread: SYSBIOS

评估板: 66AK2L06     软件:CCS8      代码在ARM Cortex-A15上

编译结果出现:Cache unsupported on device!       

检查后发现,错误是因为连接到了 C:\TI\bios_6_52_00_12\packages\ti\sysbios\family\c64p\Cache.xs;

正常应该链接到:C:\TI\bios_6_52_00_12\packages\ti\sysbios\family\arm\a15\Cache.xs;

问题在 现在不知道在哪设置的这个链接,希望大神多多指教。

.cfg 和 main 代码如下(main 只写了开头):

.cfg
/* Load all required BIOS/XDC runtime packages */
var 	Memory 		=       xdc.useModule('xdc.runtime.Memory')
var 	BIOS 		=       xdc.useModule('ti.sysbios.BIOS');
var 	HeapMem         =       xdc.useModule('ti.sysbios.heaps.HeapMem');
var 	HeapBuf         =       xdc.useModule('ti.sysbios.heaps.HeapBuf');
var 	Log 		= 	xdc.useModule('xdc.runtime.Log');
var 	Task 		= 	xdc.useModule('ti.sysbios.knl.Task');
var 	Semaphore 	=	xdc.useModule('ti.sysbios.knl.Semaphore');
var 	Hwi 		= 	xdc.useModule('ti.sysbios.hal.Hwi');
var 	ECM     	= 	xdc.useModule('ti.sysbios.family.c64p.EventCombiner');

/* Load the FFTC package */
var Fftc                        =   xdc.useModule('ti.drv.fftc.Settings');
Fftc.deviceType                 =   "k2l";
/* Load the CSL package */
var Csl     					= 	xdc.useModule('ti.csl.Settings');

/* Load the CPPI package */
var Cppi                        =   xdc.useModule('ti.drv.cppi.Settings');     

/* Load the QMSS package */
var Qmss                        =   xdc.useModule('ti.drv.qmss.Settings');

/* Device specific configuration */
var devName 					= "k2l";
Csl.deviceType 					= 	devName;

var System                      =   xdc.useModule('xdc.runtime.System');
SysStd                          =   xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy             =   SysStd;  //SysMin

/* Create a default system heap using ti.bios.HeapMem. */
var heapMemParams1              =   new HeapMem.Params;
heapMemParams1.size             =   8192 * 30;
heapMemParams1.sectionName      =   "systemHeap";
Program.global.heap0            =   HeapMem.create(heapMemParams1);

/* This is the default memory heap. */
Memory.defaultHeapInstance      =   Program.global.heap0;

Program.sectMap["systemHeap"]   =   Program.platform.stackMemory;

/****** IPC - Shared Memory Settings ********/
/* IPC packages */
var Ipc                         =   xdc.useModule('ti.sdo.ipc.Ipc');
var Settings                    =   xdc.module('ti.sdo.ipc.family.Settings');
var ListMP                      =   xdc.useModule('ti.sdo.ipc.ListMP');
var GateMP                      =   xdc.useModule('ti.sdo.ipc.GateMP');
var SharedRegion                =   xdc.useModule('ti.sdo.ipc.SharedRegion');
var HeapMemMP                   =   xdc.useModule('ti.sdo.ipc.heaps.HeapMemMP');
var MultiProc                   =   xdc.useModule('ti.sdo.utils.MultiProc');

var memmap = Program.cpu.memoryMap;

Startup = xdc.useModule('xdc.runtime.Startup');
Startup.firstFxns.$add('&myStartupFxn');

/* Configure the shared memory heap for shared memory allocations required by the
 * CPPI and QMSS Libraries */
SharedRegion.translate = false;

/* Create a shared memory heap */
MultiProc.setConfig(null, ["HOST","CORE0", "CORE1", "CORE2", "CORE3"]);

/* Synchronize all processors (this will be done in Ipc_start) */
Ipc.procSync = Ipc.ProcSync_ALL;

/* To avoid wasting shared memory for Notify and MessageQ transports */
for (var i = 0; i < MultiProc.numProcessors; i++) {
    Ipc.setEntryMeta({
        remoteProcId: i,
        setupNotify: false,
        setupMessageQ: false,
    });
}

/* Create a shared memory */
SharedRegion.setEntryMeta(0,
    { base: 0x0C010000,
      len: 0x00100000,
      ownerProcId: 0,
      isValid: true,
      name: "sharemem",
    });

/* Enable BIOS Task Scheduler */
BIOS.taskEnabled			=   true;

/*
 * Enable Event Groups here and registering of ISR for specific GEM INTC is done
 * using EventCombiner_dispatchPlug() and Hwi_eventMap() APIs
 */

ECM.eventGroupHwiNum[0] = 7;
ECM.eventGroupHwiNum[1] = 8;
ECM.eventGroupHwiNum[2] = 9;
ECM.eventGroupHwiNum[3] = 10;

/*
 *  @(#) ti.sysbios.genx; 2, 0, 0, 0,275; 4-29-2009 15:45:06; /db/vtree/library/trees/avala/avala-k25x/src/
 */

main
/* FFTC types include */
#include <fftc_types.h>

/* FFTC include */
#include <ti/drv/fftc/fftc.h>
#include <ti/drv/fftc/fftc_osal.h>

/* FFTC example application input data/ configuration files */
#include <fftc_cfg_16.h>

/* Chip Level definitions include */
#include <ti/csl/csl_chip.h>
#include <ti/csl/csl_semAux.h>
#include <ti/csl/csl_qm_queue.h>

/* PSC CSL definitions include */
#include <ti/csl/csl_psc.h>
#include <ti/csl/csl_pscAux.h>

/* CACHE CSL includes */
#include <ti/csl/csl_cache.h>
#include <ti/csl/csl_cacheAux.h>

/* XDC/BIOS includes */
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>

/* IPC includes */
#include <ti/ipc/GateMP.h>
#include <ti/ipc/Ipc.h>
#include <ti/ipc/ListMP.h>
#include <ti/ipc/SharedRegion.h>
#include <ti/ipc/MultiProc.h>
#include <ti/sysbios/knl/Task.h>
#include <xdc/runtime/Error.h>
#include <ti/sysbios/hal/Hwi.h>
#include <ti/sysbios/family/c64p/EventCombiner.h>

/* QM Accumalator firmware include */
#include <ti/drv/qmss/qmss_firmware.h>

/* Standard definitions include */
#include <string.h>

/*
 *  ======== main.c ========
 */

/*
 *  ======== taskFxn ========
 */
Void taskFxn(UArg a0, UArg a1)
{
    System_printf("enter taskFxn()\n");

    Task_sleep(10);

    System_printf("exit taskFxn()\n");

    System_flush(); /* force SysMin output to console */
}

/*
 *  ======== main ========
 */
Int main()
{ 
    Task_Handle task;
    Error_Block eb;

    System_printf("enter main()\n");

    Error_init(&eb);
    task = Task_create(taskFxn, NULL, &eb);
    if (task == NULL) {
        System_printf("Task_create() failed!\n");
        BIOS_exit(0);
    }

    BIOS_start();    /* does not return */
    return(0);
}

  • 请问是哪里看到连接到了 C:\TI\bios_6_52_00_12\packages\ti\sysbios\family\c64p\Cache.xs? plafform选对了吗?
  • 双击错误之后 发现链接到 C:\TI\bios_6_52_00_12\packages\ti\sysbios\family\c64p\Cache.xs 的, platform 选的TCI6630K2L;
    现在发现是因为 “ var ECM=xdc.useModule('ti.sysbios.family.c64p.EventCombiner'); ” 这句话才链接到 \c64p\Cache.xs的。
    程序是写在ARM上的,而EventCombiner 是为DSP服务的,我想问下这该怎么改呢? 该怎么在ARM上设置中断呢?
    ECM.eventGroupHwiNum[0] = 7; 是什么意思呢? 是不是: EventGroup[0](即 Event 4-31),对应的中断为 INT7?