采用F28M36作为主控芯片进行产品开发的过程中,发现该芯片的C核出现一定概率无法正常烧写的现象。而且一旦出现该问题后,C核只能连接但是不能再烧写。烧写时会报出如下故障:
Can’t Run Target CPU:
(Error -1156 @ 0x8050)
Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose ‘Yes’ to force the device to wake up and retry the operation. Choose ‘No’ to retry the operation without waking the device.
(Emulation package 6.0.222.0)
出现该警告后,无论点击Yes还是No,最终都会显示烧写失败。
对于类似问题,网上介绍比较多的是怀疑电源不稳的问题,但是后续通过示波器观察,并没有发现烧写前后的电压有波动的情况。
那么引起上述故障的原因会有哪些,如何避免或者修复该故障?烦请有经验的大牛们指导一下,谢谢!