如题,关于CCS6.1.3环境下VC5509A定时器中断的相关问题。
1、在6.1.3环境下,建立最简单的I/O引脚控制LED灯闪烁的程序(通过for循环延时控制亮、灭的时间),并通过XDS100v2链接自制的目标板,可实现LED闪烁功能。接下来想测试利用定时器中断来控制LED灯闪烁,结果程序编译通过,通过仿真器链接目标板运行时,怎么都进入不了中断,但通过查看Register可以看到IFR0对应定时器0的中断标志位为1。
具体程序实现思想:未采用C55XXCSL库,手动编写.cmd、vectors.asm、Tint0_Isr程序。个人感觉应该可以实现既定功能。程序代码如下所示(因程序不在本电脑上,只能传截图)。7041.docx
2,改用C55XXCSL库中example中的timer文件夹下的文件创建工程,编译通过运行暂停总是报错。如图
请有经验的开发者给予帮助。谢谢!另,由于新用6.1.3,对软件不太熟悉。6.1.3下是否只能Emulation,不能Simulation?