This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X搭配DDR3阻抗设定



AM335X datasheet写

Single-ended impedance, Zo  Typ 50Ohm,Max 75Ohm.

CK spacing set to ensure proper differential impedance. Differential impedance should be Zo x 2, where Zo is the single-ended
impedance.

DQS[x] pair spacing is set to ensure proper differential impedance. Differential impedance should be Zo x 2, where Zo is the singleended
impedance.

1.请问DQ,DQLM,ADDR,CTRL这些Single-end信号设定阻抗50Ohm,差分信号CK ,DQS[x] 的阻抗设定100Ohm,这样设定是否OK?

2.有去参考TMDSSK3358_3H0009_REV1_2A_PCB_0531.brd和BeagleBone_Black_revB6_nologo.brd,没有叠层结构(stackup impedance)无法得知具体是设定多少Ohm的阻抗,请问是否有叠构表可以参考呢?