This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在线等待高手解答关于6203B XBUS的2个问题



1.XD0-XD31上配置用的上拉、下拉电阻用多大合适?TI的数据手册中没有任何地方提到。

2.XD11配置位HMOD按TI的技术文档提示是存放在XB HPIC寄存器中的,但没有任何资料介绍该寄存器,它的地址是多少?

我们在调试6203B时发现一个很奇怪的现象需要解决上述2个问题,请高手指点,谢谢!

  • 第一个问题,芯片说明手册上没写上拉下拉的具体阻值,可以按照常规设计处理。特殊部分有阻值说明,如仿真器接口的上拉下拉均20KO。

    第二个问题看http://www.ti.com/lit/ug/spru579a/spru579a.pdf

    7.3 Expansion Bus Host Port Interface Control Register (XBHC)

  • 找到依据了:

    1.TI C6203B的数据手册没有提具体数值,且不像C6455 内部有上拉(IPU)/下拉(IPD),C6203B没有内部IPU或IPD,说明可以按常规上拉/下拉处理,例如用4.7K-20K都可以的,主要处决于XD0-XD31上连接的外部设备上拉/下拉电阻不要对正常的I/O电平有影响即可,参考EMU0的上拉值,取20K。国产的6203B开发板也是用此值。

    2.TI的SPRU190D中提到HMOD存放在XB HPIC中,这个寄存器是不存在的,即SPRU190D说法说错的,在SPRZ122A中有更正说明,其实在SPRU579A中也没这么说。