This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 nand flash boot 参数设置



6678通过EMIF连接nand flash。6678为2.0版本,按照介绍可以直接从nand flash启动。 nand flash boot时BOOTMODE[5:4]应该设置为01,即EMIF16 boot吗?

但是在EMIF16 Boot Mode Parameter Table中

14     Type       Boot only from NOR flash is supported for C6678

这是表明 nand flash boot时BOOTMODE[5:4]不能设置为01,即EMIF16 boot吗?,如果是,使用nand flash boot,那应该怎么设置BOOTMODE[12:0] 和 Boot Mode Parameter Table。

谢谢指导!