现有一块DM8127的板子,I2C1上接了一个EEPROM和加速度计mpu6050,测试发现有时候I2C1总线会出现死锁问题,软启动(reboot命令)不能复位该问题,用示波器测量发现是SDA线一直为低电平,必须得上电复位才可以,现在我用I2C1的测试功能配置SYSTEST寄存器控制CLK引脚产生9个脉冲,但是必须重试好多次才能复位,没有复位其他寄存器,后来我调用omap_i2c_init函数想复位一下所有寄存器,但是一旦执行了这个函数就会出现内核卡死现象,只能重新上电,有遇到过和我同一样问题的吗,敬请不吝指教