This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748二级引导遇到的问题



我想从spi1 flash启动,程序较大,所以做了二级引导,现在二级引导可以跑起来,但是应用程序起不来

我的工程思路是:RBL+UBL+APP(所有的代码都是在L2RAM中运行,UBL和APP通过CMD文件指定了不同的运行内存地址)

问题1:当app大于64kb时,不加UBL的情况下,RBL读取不了这么长的数据吗,导致起不来?RBL最大读取64kb的数据吗?

问题2:UBL最大是多少kb?小于等于16kb?还是小于等于64kb?

问题3:UBL利用AISgen_d800k008.exe工具生成“.ais”格式的文件,RBL会根据此文件里的一些命令初始化一些硬件环境,但是后面的APP在内存中运行时就不需要依赖RBL了吧,如果不需要依赖RBL,那么APP应该用什么工具生成什么格式的文件呢?

问题4:在UBL中我直接将APP的c_int00段的地址赋值给一个函数指针,然后调用函数指针跳转到相应的地址,这样就可以启动app了吧(当然前提是都复制到内存中去)?

问题5:在步骤4中UBL启动APP时,程序直接跑飞,PC值从APP的c_int00段的地址值开始不停的累加增长,(APP通过out2rprc.exe工具转成的".bin文件"),可以不?