This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6455 srio

专家好:

问题见附件!

问题.doc
  • PORT_OK比特没有置位可能是Serdes没有对通。如果程序和测试方法完全一样的话,需要查硬件看看Serdes上面的信号。

  • 在6678的SRIO的初始化过程也遇到类似的问题,我的是6678与switch tsi578进行互联。dsp与switch的模式,速度,时钟,都配置相同。请问YU Liu用什么办法可以进行检验Serdes上的通信信号。

  • 你好,我用6678也遇到端口没有ok的情况,这种情况出现的概率大概10%左右,多数时候还是可以通过的。请问是什么原因,怎么定位解决,谢谢

  • 你好,我用6678也遇到端口没有ok的情况,这种情况出现的概率大概10%左右,多数时候还是可以通过的。请问是什么原因,怎么定位解决,谢谢

x 出现错误。请重试或与管理员联系。