你好!我最近正在使用DM8168 EVM,我想问大家一个小白问题!我插上SD卡,sw3设置为SD卡boot模式,把sw4的nand=off,spi=off,接上串口,然后上电,是不是rom里固化的code可以自动烧写nand flash,将UBOOT拷入ram,然后启动进入bootloader引导程序,就会打印启动信息,显示TI_EVM#等类似的显示符?从SD卡启动,除了上述步骤,我还要不要自己往flah烧写程序?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SD卡启动模式的设置请参照文档说明。
另外,SD启动不会往flash里烧写uboot的,在SD启动成功后,需要自己往flash里烧写程序。比如烧写uboot到nand flash,之后可以选择nand flash启动了。
您好 :
我现在正在使用8168产品,但是现在遇到一些问题,希望您能给与一些建议,首先就是MCFW架构,在Ti给的demo中没有找到关于ARM和DSP通信的例程,我们想做的就是在ARM端调用DSP的算法,不知道这个里面有没有类似与之前的CodecEngine的东西,使二者能够结合工作,还有他们说在运动检测的demo中有关于M3和DSP的通信 但是我没有找到相关的例程,所以想知道他们之间是怎样实现通信的,谢谢您!!!