This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713B使用过程中的HPI操作问题



问题1

       在使用CPLD进行写HPI操作时发现,偶尔会使得DSP的RAM数据区内被写入数据00003E66,有时候是连续出现在RAM中,有时候会隔几个00000000周期出现。请问这是什么操作导致的?

问题2

       请问C6713B的HPI接口在工作过程中有没有哪种错误模式会导致HPI读写功能完全失效?

       系统采用的是CPLD+DSP的设计方案,CPLD作为host,通过HPI对DSP的RAM进行读写。按照一定周期进行循环工作,采取先读后写的方式,然而在上电的时候有几率(大约70-80次出现一次)出现输出数据异常的情况,这个时候通过CCS对DSP的指定RAM数据区进行观察,没有任何数据写入更新,读出的数据与特定RAM数据区的数据也不一样,初步判断时HPI功能已经失效,(至少)无法完成对指定地址数据的读写操作,需要再次上电重启或在连接CCS的情况下使用CCS对DSP进行复位才能恢复。

       分析推测产生的原因是上电最初的一个周期时间长度不稳定,短于正常的周期,使其在HPI的读写操作过程被打断,CPLD提前进行了复位并开始下一个周期的循环。