TI的DM816X/AM389X开发板,SD卡启动后进入U-BOOT命令行模式,通过setenv ipaddr设置IP地址,ubuntu主机端设置好同一网段IP,从开发板PING主机,打印信息using davinci emac device,host 192.168.0.160 is alive。主机端PING开发板PING不通,但是可以通过TFTP下载程序到开发板。用同一根网线连接ubuntu主机和另一台winxp主机,可以PING通,请问可能是什么原因,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的DM816X/AM389X开发板,SD卡启动后进入U-BOOT命令行模式,通过setenv ipaddr设置IP地址,ubuntu主机端设置好同一网段IP,从开发板PING主机,打印信息using davinci emac device,host 192.168.0.160 is alive。主机端PING开发板PING不通,但是可以通过TFTP下载程序到开发板。用同一根网线连接ubuntu主机和另一台winxp主机,可以PING通,请问可能是什么原因,谢谢