This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何利用ti的g.726程序移植到5505的DSP上



在ti上获取了g.726的安装程序

但是readme中说实在ccs2的版本上运行。我用的是ccs6,请问如何才能在ccs6上使用这个文件下的代码,我该如何移植?谢谢!

  • 不能直接import到ccsv6, 在ccsv6中新建工程。
  • 嗯谢谢!
    有几个问题:
    1、请问需要先用make编译文件吗?ti提供的文件夹中的readme中提到了用make构建ccs2的程序,我们仅仅只需要其源码,请问还需要编译吗?
    2、在ti提供的文件夹中,仅仅在tstsrc文件中有一些测试程序,在其他文件中,只有一些.h头文件,请问我们是不是只能从测试文件中获取我们想要的代码吗?
    3、我们希望在5505上使用乒乓操作,实现实时的g.726编解码,请问这个可行吗?因为ti提供的测试程序中,使用 方法都是从文件中读取写入,不知道是否在实时条件下也可以,还是我们必须再在这个基础上做一些优化?(改成汇编?循环展开?)
    希望能得到你们的回复,非常感谢!!!