This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

当我用gstreamer视频解码时遇到了CMEMK Error: Failed to find a pool which fits 1843200错误,



用的DM368,当我用gstreamer视频解码时遇到了CMEMK Error: Failed to find a pool which fits 1843200错误,打印信息如下

Pipeline state changed from NULL to READY:
dynamic_addpad In dynamic ADDING PAD
dynamic_addpad In dynamic ADDING PAD2
[ 124.310000] CMEMK Error: Failed to find a pool which fits 1843200
CMEM Error: getPool: Failed to get a pool fitting a size 1843200
Failed to allocate memory.
Segmentation fault

请问这是分的pool不够吗?第一次遇到这个问题,调试时间不长,有点无从下手

在视频编码时也遇到过问题   修改了bootargs  后可以编码了     

谢谢啦