This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x SPI数据波形

我在用AM335x EVM裁剪的板子,经过大家的帮忙,移植上了linux系统,添加了SPI设备,可是现在的问题是SPI的输出只有片选和时钟有波形,数据没有波形,我输出了好长时间的数据,决定不是时间不够的问题,请大家帮忙分析下问题大概在哪里,我是这样改的board-am335xevm.c。

增加:

static struct spi_board_info am335x_spi0_info[] = {
{
.modalias = "spidev",
.max_speed_hz = 48000000, //48 Mbps
.bus_num = 1,
.chip_select = 0,
.mode = SPI_MODE_1,
},
};

改了下:

static void spi0_init(int evm_id, int profile)
{
setup_pin_mux(spi0_pin_mux);
spi_register_board_info(bone_spi0_info,
ARRAY_SIZE(am335x_spi0_info));
return;
},

在结构体了添加{spi0_init, DEV_ON_BASEBOARD, PROFILE_ALL},

然后在内核配置的时候,选了User mode SPI device driver support,这样编译出来就有dpidev了。

可是为什么没有数据波形呢,求助