This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6748 NDK2.00使用中断的问题



各位好:

        我使用的是C6748做网络发送接收,用的NDK版本是2.00,现在发现NDK用了DSP的INT5和INT6,而我要用两个HWI,所以只能一个放在INT4上一个在INT7上,然后我发现当NDK运行之前我的两个中断都能响应,但是一旦NDK运行之后INT7的中断就无法响应,我现在想把NDK的中断优先级改低一点,但是在代码上都找不到怎么改,各位有这种经验的帮帮忙吧!

        谢谢!