This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA7xx Issue:在按照Processor SDK Linux Automotive Software Developers Guide中的【Building Yocto Filesystem】编译sdk时,编译错误

各位:

在按照Processor SDK Linux Automotive Software Developers Guide中的【Building Yocto Filesystem】编译sdk时,编译出错。

具体步骤是:

1.export INSTALL_DIR="${HOME}/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf"

2.export PATH=/home/linux/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf/bin:$PATH

3.cd $INSTALL_DIR

4. ./bin/setup-yocto.sh

5.cd yocto-layers

6. ./build-core-sdk.sh dra7xx-evm

=========================================================================================================

执行最后一步时,编译提示ERROR: Function failed: Unpack failure for URL: 'libloki.sourcearchive.com/.../libloki_0.1.7.orig.tar.gz'.

整个log的内容

DEBUG: Executing python function do_unpack

DEBUG: Executing python function base_do_unpack

NOTE: Unpacking /home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/downloads/libloki_0.1.7.orig.tar.gz to /home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/libloki/0.1.7-r0/

gzip: stdin: not in gzip format

tar: Child returned status 1

tar: Error is not recoverable: exiting now

DEBUG: Python function base_do_unpack finished

DEBUG: Python function do_unpack finished

ERROR: Function failed: Unpack failure for URL: 'libloki.sourcearchive.com/.../libloki_0.1.7.orig.tar.gz'. Unpack command PATH="/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/sources/oe-core/scripts:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/arm-linux-gnueabi:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/dra7xx-evm/usr/bin/crossscripts:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/home/linux/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf/bin:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/sources/oe-core/scripts:/home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/sources/bitbake/bin:/home/linux/gcc-linaro-5.3-2016.02-x86_64_arm-linux-gnueabihf/bin:/home/linux/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games" tar xz --no-same-owner -f /home/linux/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/downloads/libloki_0.1.7.orig.tar.gz failed with return value 2

Building Yocto Filesystem

x 出现错误。请重试或与管理员联系。