当前的配置和状态是这样的:
1、配置03寄存器,配置BIT2为1,即使能TCHEN,使能风扇转速统计
2、配置转速门限,即0x49_0x48寄存器的值为500
3、统计到转速的值,即0x47_0x46寄存器的值为4000多
4、读取02告警寄存器,bit0的值为1,即有Tach Alarm(该bit描述:When this bit is a 1, the Tachometer count is higher than the Tachometer Limit
(the RPM of the fan is less than the minimum desired RPM), and an ALERT is triggered)
5、16H寄存器的alert mask,TCHAM的值为0,使能该告警(该bit描述:When this bit is a 0, a Tach Alarm event will generate an ALERT.)
综合以上信息来看,有alert告警了,也使能告警触发alert,但是量器件的alert管脚,始终为高电平的状态;修改转速门限大于转速,告警消失,但是alert管脚的电平始终不变。哪位用过这个器件,是什么原因?谢谢