This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9222+UCD7242的问题

Other Parts Discussed in Thread: UCD9222, UCD7242

我们现在打算做一块C6678的板子,才刚开始就遇到问题了

参考C6678的EVM,使用UCD9222+UCD7242给C6678 提供DVDD scaled、DVDD1V fixed这两个电压的。

再参考了UCD9222的相关资料之后,达县UCD9222需要通过PMBUS对其进行编程。

我想问的是:

1. 如果这两个电压完全按照EVM的设计来做的话,是不是可以直接用advantech提供的Fusion Digital Power Designer软件的xml文件,直接用这配置文件烧写UCD9222?

2. 要烧写UCD9222的话,是不是还得要带上TI的USB-to-GPIO小板子?

3. EVM上UCD9222的PMBUS接口为什么连接到FPGA?按照EVM手册上说的,是不是RFU,就是说不将UCD9222的PMBUS连接FPGA也行?直接留出来,通过TI的USB-to-GPIO连接PC,烧写文件,即可?

4. EVM上还用到了UCD9222的JTAG接口,请问这么做是什么目的?

5. 关于C6678的DVDD scaled、DVDD1V fixed电压的设计,有没有其他简单、方便设计的替代方案?

因为我总感觉UCD9222+UCD7242这么做,貌似太麻烦了,我打开了Fusion Digital Power Designer那个软件,头都大了,好多要设置的。。。。对于C6678最小系统相关的设计,应该最简单、最容易实现为上吧。。。有了最小系统的话,在其上再做设计就好办了。

希望TI的FAE专家能给我解答。非常感谢!!