This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385低温启动电流偏大

Other Parts Discussed in Thread: TPS54394

hi:

      论坛的大佬,我们最近一个图像板使用DM385AAARD21F,芯片工作温度-40-95℃,我们的供电使用TI的TPS54394,上电时序严格按照时序要求,有FPGA控制,在常温时,工作正常,

现在在-20℃环境下,存储2小时,开机后,发现图像板的功耗会比常温工作时大3.6W,功能是正常的,测量各路供电电压,也是正常的,我们的器件工作温度都是能到-40℃,当单板运行一段时间,板子温度升上去了,功耗也没有恢复正常,如果断电重启单板,图像板板功能正常,功耗也正常了,  请教下,可能是什么原因会导致DM385低温启动功耗偏大?

  • 你好,

    请问你的功耗是如何测量的?测量的是图像板电源输入,例如12V输入侧的功耗么?

    你能否在-20度开机的时候,使用红外温枪看板上各部分的温升,对比正常情况下的,找到功耗消耗的最大点和不同点。我手上只有DM814x的功耗估计表格,从表格信息看,环境温度越低功耗应该比常温要低。
  • 是的,我估算功耗看的是12V电流,低温启动的时候,电流比常温工作大了0.3A, 目前没有温枪可以测试温度点,我想办法确定到底是哪部分电流变大了