This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X如何用DM9000扩展出第三路以太网



AM335X本来支持两路以太网,现在想做成3路以太网,想用DM9000去扩展一路网络,AM335X只外接了RAM,flash,调试串口这些基本核心,现在还空出很多引脚,主要有一些GPIO引脚,请问大家DM9000是否可以接到AM335X的GPIO上,然后通过操作GPIO的寄存器就可以用DM9000;或者像S3C2440那样DM9000接到数据线上,通过片选分开RAM,nandflash和DM9000,但是AM335X已经将RAM和flash的数据线分开了,没用共用数据线;请各位出出主意,DM9000到底怎样连接到AM335X才合理。谢谢大家!