This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教HaiGun Guo老师,在DM8148 DVRRDK2.80中如何将H264码流与IPCBITS_HLOSOUT(host)link链接起来?



老师你好!

        我想要实现的功能是将来自网络的H264视频码流交给DEC本地显示,不知道怎么将H264码流数据通过IPCBITS_HLOSOUT(host)LINK给IPCBITS_RTOSIN(VID)LINK。希望可以得到一些提示。我参考的是dvrrdk2.8里面的demo_vdec_vdis.c ,demo_vdec_vdis_frames_send.c,multich_vdec_vdis.c用例,其中有两个函数VdecVdis_ipcFramesCreate()和VdecVdis_ipcFramesStart(),大概是什么作用?

  • 参考的demo没错,不过将码流送给VID的部分在文件 demo_vdec_vdis_bits_rd.c中,而不是demo_vdec_vdis_frames_send.c。

    VdecVdis_ipcFramesCreate()和VdecVdis_ipcFramesStart(),是用来创建VideoM3和VpssM3之间传递解码后数据的通路。