看DM368的DataSheet,其USB2.0可以达到480Mbps
但是,通过测试,发现只能达到64Mbps,
不知道有没有专门研究过DM368的USB,是只能到这么多么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看DM368的DataSheet,其USB2.0可以达到480Mbps
但是,通过测试,发现只能达到64Mbps,
不知道有没有专门研究过DM368的USB,是只能到这么多么?
我将DM368设成Slave,建立一个ISO的Endpoint,packetsize设成1024,PC端进行接收。DM368往PC端发送数据,这个过程纯粹进行数据的发送/接受,没有任何写外存的操作。测出来的结果是每秒大约8MB,USB2.0的理论速度应该是60MB。这种差距就太大了,所以想咨询一下TI专家的意见。
我看了DM368的PSP性能测试报告, "USB Slave-DMA-Write Performance values"里面写DM368的Data Rate是8.9MB(我不明白的是,既然DM368作为Slave,怎么还有"Bytes Transferred (MB)'MicroSD Trascend as storage device'"这样的条件?)。
现在的情况是,我们的应用需要USB的速度至少能达到30MB,有没有什么办法进行改进?