我们现在在设计车载智能DVR的方案,用于图像目标识别,比如特定车辆、行人等,但是我感觉一个双核Davinci(DM8148、DM8168)处理能力不够,打算用DM8148(linux系统)作为视频编解码、录像以及控制,然后通过PCIe把解码后的720P数据传输给C6678,经过多核处理器处理后,把识别情况反馈给DM8148,不知道我这个方案可行与否?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
硬件框架中需要注意的是数据传到DSP,经过处理再传回8148的时延。是否有需要和8148上的数据流保持同步?
如果同步上没有问题,这个框架合理的。
我这里没有看出什么问题。
另外,为什么要将解码后的YUV传送到6678呢?将采集下来的(编码之前的)YUV送到6678不可以吗?是否没有这个需求?只在回放录像时才需要6678进行算法分析?
C6678相关的问题不清楚,DM8148上的流程在DVR RDK中,绝大部分数据流都有现成的usecase文件供参考。需要自己添加的就是通过PCIE传递数据,这部分也应该是A8应用侧做的,所以DM8148上的数据流可以直接参照DVRRDK,C6678上的算法也可以独立同步开发,重点在于定义和实现DM8148与C6678之间的接口。