This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCASP在NandFlash方式运行时,只输出0



大家好:

我再使用OMAPL138(只使用了DSP核,ARM处于复位状态)输出音频时,在DEBUG模式下,输出完成正常,但是我把程序烧录到Nand,从Nand启动时,发现输出全部是0(我使用的是I2S的从机模式,位时钟和通道切换时钟由外设提供)。

通过我接的一个LED可以看出处理器已经正常工作,同时连接MCASP的EDMA也正常中断(也是通过LED的闪烁频率来判断的)。