This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358使用USB Camera,视频画面非常卡顿

Other Parts Discussed in Thread: AM3358

大家好,

1.目前BSP包移植米尔科技的,内核版本为L4.1.18,暂不确定对应为TI的哪个版本SDK。

2.在使用USB Camera时,使用QT程序查看视频,画面非常卡顿,延迟很久,且CPU占用率高达100%,目前暂不知道是哪里的问题?

3.在使用一个Demo程序,采集Camera数据后,直接用framebuffer显示,在am3358上视频图像无法正常显示,且画面异常卡顿,有时延迟高达12s。使用同样的程序,在freescale的imx6solo上运行,视频图像可以正常显示,且延时仅在500ms内。

对于以上问题,初步怀疑是TI这边有问题,可能是芯片bug,也可能是SDK问题。

在查看论坛时有提到为SDK bug,请问这个问题现在有结果了吗?

谢谢