如后面的图,主要有两个错误:
[ 0.000000] Hit pending asynchronous external abort (FSR=0x00001211) during first unmask, this is most likely caused by a firmware/bootloader bug.
和
[ 0.396229] WARNING: CPU: 0 PID: 1 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x254/0x370
[ 0.396240] 44000000.ocp:L3 Custom Error: MASTER MPU TARGET L4_CFG (Read): Data Access in User mode during Functional access
[ 0.396247] Modules linked in:
[ 0.396263] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.14.79-gbde58ab01e #3
我们自己的板子很多功能有裁剪的,这两个错误让我无从查起,不知道是设备树的哪一块没有配置或者没配置好