This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 SRIO LSU_state_index_table



请教下,SRIO例子代码,LSU_state_index_table 列表是什么含义?

  • 这个索引表的含义,请参考下面附件文档第30页。

    The LSU transfer completion is checked through LSU_STAT_REG registers. The transaction ID
    read from LSU_REG6 is used to determine the index of the completion code in
    LSU_STAT_REG registers; the context bit read from LSU_REG6 is used to determine the
    validation of the completion code. The context bit toggles for each transaction, for example, for
    the first transfer with transaction ID = 2, the context bit = 1; then, for the next transfer with
    transaction ID = 2, the context bit = 0. So, only after the context bit in LSU_STAT_REG register
    for transaction ID = 2 toggles from 1 to 0, it indicates the second transfer complete, and the
    completion code is valid. Below is the example code for LSU completion checking.

    2045.SRIO_Programming_Performance.pdf