This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 doorbell 信号



  1. 6657在directio模式下,用寄存器组LSUx_Regx配置数据的发送,可以用Drbll_val位配置发送完成后是否发送doorbell信号,但是无法配置Drbll Info值,这个值只有在包类型FType为10(即doorbell包),才有效;
  2. 如果在FType为SWRITE,并且配置了发送完成后发送doorbell信号(Drbll_val位置1),则Drbll Info(包类型FType不为10)信号因为无法配置,发送给对方的是多少呢?
  3. SWRITE发送完成后,发送的doorbell信号是否需要响应也没有寄存器可配置,是否就是由包类型决定?
  4. 在directio模式,对方发送了一个doorbell信号给6657,如果是需要RESPONSE包,6657怎么响应呢,是否需要在中断里发送一个什么包给对方,还是芯片SRIO模块自动完成响应包的发送,在例子工程中没看到这部分代码,只有响应中断。