This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678存储器相关疑问



在学习多核DSP 6678时,突然产生了一个疑问,就是如果DSP6678中只使用一个内核,那么其他内核的L1,L2存储单元能够提供给使用的那个内核作为存储数据或者程序吗?

说明:每一个内核的L1和L2都有一个全局地址。比如说在Debug时,Core0是加载了程序的,Core1-7均为加载程序,仅仅进行了初始化(采用gel文件),那么Core0在运行过程中,可否操作Core1-7的L1或者L2存储区时?