This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 ENET_ECHO例程烧写后网络起不来

C6748 的CMD中区都是放在DDR2中,ENET_ECHO例程烧写到NOR或NAND都没问题,网络正常。

发现运行速度慢,尝试CMD修改放到RAM中运行,仿真器可以跑,但是烧写到NOR或NAND后网络都起不来(创龙开发板)。

求助有办法或有尝试过的吗?

  • 将CMD修改到RAM上的时候请按以下帖子里method1提供的CMD文件修改并烧写。
    e2e.ti.com/.../439030
  • 您好,感谢您的回复,如您所说将如下CMD加入工程,仿真器运行ENET_ECHO原始工程,采用静态IP,网络连接不上,改回原来CMD可以。
    然后烧写到NOR中测试,同样网络连接不上。

    请问有没有其他需要注意的项?






    //C6748_RAM.cmd
    // ============================================================================
    
    // Linker Command File for Linking c674 DSP Programs
    
    //
    
    // These linker options are for command line linking only. For IDE linking,
    
    // you should set your linker options in Project Properties.
    
    //         -c                    Link Using C Conventions
    
    //        -stack     0x1000        Software Stack Size
    
    //        -heap    0x1000        Heap Area Size
    
    // ===========================================================================
    
    -stack 0x1000
    
    -heap 0x1000
    
    // ============================================================================
    
    //                         Specify the System Memory Map
    
    // ============================================================================
    
    MEMORY
    
    {
    
       L1P:    o = 0x11E00000        l = 0x00008000
    
       L1D:    o = 0x11F00000        l = 0x00008000
    
       L2:     o = 0x11800000        l = 0x00040000
    
       DDR:   o = 0xC0000000        l = 0x08000000
    
    }
    
    // ============================================================================
    
    //                 Specify the Sections Allocation into Memory
    
    // ============================================================================
    
    SECTIONS
    
    {
    
       .cinit        >        L2               // Initialization Tables
    
       .pinit        >        L2               // Constructor Tables
    
       .init_array   >        L2               //
    
       .binit        >        L2               // Boot Tables
    
       .const        >        L2               // Constant Data
    
       .switch       >        L2               // Jump Tables
    
       .text         >        L2               // Executable Code
    
       .text:_c_int00: align=1024 > L2         // Entrypoint
    
       GROUP (NEARDP_DATA)                       // group near data
    
       {
    
          .neardata
    
          .rodata
    
          .bss                                   // note: removed fill = 0
    
       }             >        L2
    
       .far: fill = 0x0, load > L2             // Far Global & Static Variables
    
       .fardata      >        L2               // Far RW Data
    
       .stack        >        L2               // Software System Stack
    
       .sysmem       >        L2               // Dynamic Memory Allocation Area
    
       .cio          >        L2               // C I/O Buffer
    
       .vecs         >        L2               // Interrupt Vectors
    
    }

  • 您好,感谢您的回复,如您所说将如下CMD加入工程,仿真器运行ENET_ECHO原始工程,采用静态IP,网络连接不上,改回原来CMD可以。
    然后烧写到NOR中测试,同样网络连接不上。

    请问有没有其他需要注意的项?






    //C6748_RAM.cmd
    // ============================================================================

    // Linker Command File for Linking c674 DSP Programs

    //

    // These linker options are for command line linking only. For IDE linking,

    // you should set your linker options in Project Properties.

    // -c Link Using C Conventions

    // -stack 0x1000 Software Stack Size

    // -heap 0x1000 Heap Area Size

    // ===========================================================================

    -stack 0x1000

    -heap 0x1000

    // ============================================================================

    // Specify the System Memory Map

    // ============================================================================

    MEMORY

    {

    L1P: o = 0x11E00000 l = 0x00008000

    L1D: o = 0x11F00000 l = 0x00008000

    L2: o = 0x11800000 l = 0x00040000

    DDR: o = 0xC0000000 l = 0x08000000

    }

    // ============================================================================

    // Specify the Sections Allocation into Memory

    // ============================================================================

    SECTIONS

    {

    .cinit > L2 // Initialization Tables

    .pinit > L2 // Constructor Tables

    .init_array > L2 //

    .binit > L2 // Boot Tables

    .const > L2 // Constant Data

    .switch > L2 // Jump Tables

    .text > L2 // Executable Code

    .text:_c_int00: align=1024 > L2 // Entrypoint

    GROUP (NEARDP_DATA) // group near data

    {

    .neardata

    .rodata

    .bss // note: removed fill = 0

    } > L2

    .far: fill = 0x0, load > L2 // Far Global & Static Variables

    .fardata > L2 // Far RW Data

    .stack > L2 // Software System Stack

    .sysmem > L2 // Dynamic Memory Allocation Area

    .cio > L2 // C I/O Buffer

    .vecs > L2 // Interrupt Vectors

    }
x 出现错误。请重试或与管理员联系。