This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148-M114(DM8127 IPNC Rev 0.6)IPNC无法通过网页浏览器链接进去使用



我使用的软件是TI提供的IPNC_RDK_GA_V3.2.0,在ubuntu按照好交叉编译后能成功make出(两个uboot,和uImage、文件系统ubifs),按照TI提供的IPNC Installation 更新Uboot和内核、文件系统。启动机器后,

./bin/ipnc_rdk_mcfw.out   TRISTREAM TRIPLE_H264 TI2A AEWB 1080P_D1 H264 HIGH_SPEED1 H264 HIGH_SPEED2 MJPEG 80 &

这个IPNC _RDK进程已经跑起来了。但是按照那个IPNC Installation说明书无法通过浏览器来访问它,求帮忙解决!!!

下面是一些开机启动时发现的错误提示信息:

 sbulla: unknown partition table  

  [m3vpss ]  63VFS: Can't find a valid FAT filesystem on dev sbulla.

 VFS: Can't find a valid FAT filesystem on dev sbulla.

mkdosfs 2.11 (12 Mar 2005)

unable to get drive geometry, using default 255/63/dev/sbulla has 255 heads and 63 sectors per track,

logical sector size is 512,

using 0xf8 media descriptor, with 1024 sectors;

file system has 2 12-bit FATs and 4 sectors per cluster.

FAT size is 1 sector, and provides 247 clusters.

Root directory contains 512 slots.

Volume ID is 4d821b68, no volume label.