This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL-138 dsplink加载成功,但是不好使

Other Parts Discussed in Thread: OMAP-L138

我在omapl138上开发的dsplink,在davinci-psp-sdk-0.3.20.00.06下可以实现dsplink的例程readwrite,但是在davinci-psp-sdk-0.3.22.00.02下实现readwrite出错,错误如下:

 

root@da850-omapl138-evm:/usr/dsplinktestaddconfigfor22.00.02# ./readwritegpp rea
dwrite.out 0xC3F5B000 1024 1000
============= Sample Application : READWRITE ==========
Entered RDWR_Create ()
copy_from_user call failed 24
PROC_setup failed. Status: [0x80008008]
Leaving RDWR_Create ()
Create phase failed. Status: [0x80008008]
Entered RDWR_Delete ()
Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 478
MSGQ_release () failed. Status = [0x8000800b]
MSGQ_transportClose () failed. Status = [0x80008002]
Assertion failed (IS_VALID_MSGQ (msgqQueue)). File : msgq.c Line : 329
Leaving RDWR_Delete ()
=======================================================

怎么回事?请大家帮帮忙