我使用的DM3730的板子是beagleboard-xm,我想知道关于这个板子,是否可以使用TI官方的wiki上的资料,如果可以使用,希望给出网址的链接
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你是否做android2.3系统?如果是android系统,无论是Mistral的板子,还是Beagleboard的板子,都是一套系统。
这里有对beagleboard-xm的介绍:看一下链接,有linux\wince\android的链接。:
http://en.wikipedia.org/wiki/BeagleBoard#BeagleBoard-xM
Beagleboard的官方网站上也有:http://beagleboard.org/project/rowboat/ :有问题,可联系QQ: 315676522
BeagleBoard-xM
Features
-xM board
A modified version of the BeagleBoard called the BeagleBoard-xM started shipping on August 27, 2010. The BeagleBoard-xM measures in at 82.55 by 82.55 mm and has a faster CPU core (clocked at 1 GHz compared to the 720 MHz of the BeagleBoard), more RAM (512 MB compared to 256 MB), onboard Ethernet jack, and 4 port USB hub. The BeagleBoard-xM lacks the on board NAND and requires the memory and OS to be stored on to a microSD card. The addition of the Camera port to the -xM provides a simple way of importing video via Leopard Board cameras.[17][18]
Specifications
Package on Package POP CPU/memory chip.
Processor TI DM3730 Processor - 1 GHz ARM Cortex-A8 core
'HD capable' TMS320C64x+ core (800 MHz up to 720p @30 fps)[6]
Imagination Technologies PowerVR SGX 2D/3D graphics processor supporting dual independent displays[5]
512 MB LPDDR RAM memory[6]
4 GB microSD card is supplied with the BeagleBoard -xM loaded with Angstrom.
Peripheral connections[7]
DVI-D (HDMI connector chosen for size - maximum resolution is 1280×1024)
S-Video
USB OTG (mini AB)
4 USB ports
Ethernet port
MicroSD/MMC card slot
Stereo in and out jacks
RS-232 port
JTAG connector
Power socket (5 V barrel connector type)
Camera port
Expansion port
Development[8]
Boot code stored on the uSD card
Boot from uSD/MMC only
Alternative Boot source button.
Has been demonstrated using Android[9], Angstrom Linux[10], Fedora, Ubuntu, Gentoo[11] and Maemo Linux distributions[12], the Windows CE operating system[13].