This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6657 cache操作



请教如下问题

1. 在进行cache一致性操作时。

内存块写回函数WritebackInvalidCache(void * blockPtr, Uint32 byteCnt)

一次最大只能对256k(0xFFFF*4)的空间进行写回操作,如果缓存较大为1024K,是否需要多次调用该函数,然后基地址进行累加。
假设我的缓存空间在DDR中,起始地址baseaddr=0x80000000,,大小为1024K,是否需要如下写法:

for(i=0;i<4;i++)

{

WritebackInvalidCache(baseaddr+1024*256*i, 1024*256);

}

即调用4次,每次累加,或者把cache空间做全部失效处理。