我在跑自己写的helloworld以及CCS自带的6678的例子时
可以进行单步调试,但过程中多次出现
Can't find a source file at "/db/rtree/library/trees/xdcprod/xdcprod-q45/product/Linux/xdctools_3_24_05_45_eng/packages/xdc/runtime/Core-params.c"
Locate the file or edit the source lookup path to include its location.
这类问题
并且点击运行,也会报错
Can't find a source file at "/tmp/TI_MKLIB6sLCzz/SRC/exit.c"
Locate the file or edit the source lookup path to include its location.
我按照网上说的blog.csdn.net/.../3747384
- From the editor error page, select the "Edit Source Lookup Path..." button and select the "Add..." button
- Or, in the eclipse IDE, go to menu Window -> Preferences -> C/C++ -> Debug-> Common Source Lookup Path -> Add.
- From the list of lookup containers, choose Path Mapping and OK. You get a New Mapping in the list.
- Select the mapping and then Edit. In the Modify the path mappings dialog, select Add, and then enter:
- /cygdrive/c as the compilation path and
- c:/ as the local file system path.
- Select OK, OK, OK to finish the dialogs.
- Terminate the debug session and restart; it should find your source files now 设置了映射路径,错误依然存在,请大家帮帮忙,非常感谢