This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NFS挂载根文件系统问题



TI的AM389X/TI816X开发板,用的自带的SD卡u-boot引导SD卡里内核后,通过NFS可以挂载根文件系统,通过SD卡里u-boot启动后通过tftp下载EZSDK里prebuild的uimage-dm816x-evm.bin后,NFS挂载根文件系统出错,自己重新编译内核(根据EZSDK里的816x开发板的默认配置),结果一样不行,请问可能是什么原因,可能是内核哪个部分配置有问题呢,都是EZSDK提供的,为什么有的行有的不行

  • 能否贴出log信息?

  • 一下是从SD卡启动后,进入u-boot命令行后,通过TFTP下载内核(uImage-dm816x-evm.bin)到内存0x81000000,bootm 0x81000000后的信息

    环境变量设置为:ipaddr 192.168.0.12

                                    serverip 192.168.0.11

                                   bootargs= "console=ttyO2,115200n8 noinitrd init=/linuxrc root=/dev/nfs nfsroot=192.168.0.11:/home/sony/targetfs,nolock rw nfsrootdebug mem=128M ip=192.168.0.12:192.168.0.11:192.168.0.1:255.255.255.0::eth0:off "

    ## Booting kernel from Legacy Image at 81000000 ...
    Image Name: Arago/2.6.37-psp04.04.00.01/dm81
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 2563384 Bytes = 2.4 MiB
    Load Address: 80008000
    Entry Point: 80008000
    Verifying Checksum ... OK
    Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    Linux version 2.6.37 (x0029463@swubn01) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Sun Apr 29 20:16:23 IST 2012
    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
    Machine: ti8168evm
    reserved size = 52428800 at 0x0
    FB: Reserving 52428800 bytes SDRAM for VRAM
    Memory policy: ECC disabled, Data cache writeback
    OMAP chip is TI8168 2.0
    Built 1 zonelists in Zone order, mobility grouping on. Total pages: 19712
    Kernel command line: console=ttyO2,115200n8 noinitrd init=/linuxrc root=/dev/nfs nfsroot=192.168.0.11:/home/sony/targetfs,nolock rw nfsrootdebug mem=128M ip=192.168.0.12:192.168.0.11:192.168.0.1:255.255.255.0::eth0:off
    PID hash table entries: 512 (order: -1, 2048 bytes)
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 78MB = 78MB total
    Memory: 73224k/73224k available, 57848k reserved, 0K highmem
    Virtual kernel memory layout:
    vector : 0xffff0000 - 0xffff1000 ( 4 kB)
    fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
    DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
    vmalloc : 0xc8800000 - 0xf8000000 ( 760 MB)
    lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
    pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
    modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
    .init : 0xc0008000 - 0xc003b000 ( 204 kB)
    .text : 0xc003b000 - 0xc04d8000 (4724 kB)
    .data : 0xc04d8000 - 0xc0520f00 ( 292 kB)
    SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    NR_IRQS:407
    IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    Total of 128 interrupts on 1 active controller
    GPMC revision 6.0
    Trying to install interrupt handler for IRQ400
    Trying to install interrupt handler for IRQ401
    Trying to install interrupt handler for IRQ402
    Trying to install interrupt handler for IRQ403
    Trying to install interrupt handler for IRQ404
    Trying to install interrupt handler for IRQ405
    Trying to install interrupt handler for IRQ406
    Trying to install type control for IRQ407
    Trying to set irq flags for IRQ407
    OMAP clockevent source: GPTIMER1 at 27000000 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)
    pid_max: default: 32768 minimum: 301
    Security Framework initialized
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    devtmpfs: initialized
    omap_voltage_early_init: voltage driver support not added
    regulator: core version 0.5
    regulator: dummy:
    NET: Registered protocol family 16
    omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting!
    omap_voltage_add_dev: VDD specified does not exist!
    OMAP GPIO hardware version 0.1
    OMAP GPIO hardware version 0.1
    omap_mux_init: Add partition: #1: core, flags: 0
    _omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl
    _omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda
    NOR: Can't request GPMC CS
    registered ti816x_gpio_vr device
    registered ti816x_sr device
    pm_dbg_init: only OMAP3 supported
    registered ti81xx_vpss device
    registered ti81xx_vidout device
    registered ti81xx on-chip HDMI device
    registered ti81xx_fb device
    registered ti81xx_vin device
    ti81xx_pcie: Invoking PCI BIOS...
    ti81xx_pcie: Setting up Host Controller...
    ti81xx_pcie: Register base mapped @0xc8820000
    ti81xx_pcie: Starting PCI scan...
    PCI: bus0: Fast back to back transfers enabled
    bio: create slab <bio-0> at 0
    regulator: VFB: 800 <--> 1025 mV at 1010 mV
    vgaarb: loaded
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    USBSS revision 4ea20809
    registerd cppi-dma Intr @ IRQ 17
    Cppi41 Init Done
    omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
    omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
    Advanced Linux Sound Architecture Driver Version 1.0.23.
    Switching to clocksource gp timer
    musb-hdrc: version 6.0, host, debug=0
    musb-hdrc musb-hdrc.0: dma type: dma-cppi41
    MUSB controller-0 revision 4ea20800
    musb-hdrc musb-hdrc.0: MUSB HDRC host driver
    musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb1: Product: MUSB HDRC host driver
    usb usb1: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb1: SerialNumber: musb-hdrc.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    musb-hdrc musb-hdrc.0: USB Host mode controller at c881e000 using DMA, IRQ 18
    musb-hdrc musb-hdrc.1: dma type: dma-cppi41
    MUSB controller-1 revision 4ea20800
    musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
    usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb2: Product: MUSB HDRC host driver
    usb usb2: Manufacturer: Linux 2.6.37 musb-hcd
    usb usb2: SerialNumber: musb-hdrc.1
    hub 2-0:1.0: USB hub found
    hub 2-0:1.0: 1 port detected
    musb-hdrc musb-hdrc.1: USB Host mode controller at c8826800 using DMA, IRQ 19
    NET: Registered protocol family 2
    IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
    TCP established hash table entries: 4096 (order: 3, 32768 bytes)
    TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    NetWinder Floating Point Emulator V0.97 (double precision)
    PMU: registered new PMU device of type 0
    omap-iommu omap-iommu.0: ducati registered
    omap-iommu omap-iommu.1: sys registered
    JFFS2 version 2.2. (NAND) ?? 2001-2006 Red Hat, Inc.
    msgmni has been set to 143
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0
    omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    console [ttyO2] enabled
    brd: module loaded
    loop: module loaded
    ahci ahci.0: forcing PORTS_IMPL to 0x3
    ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode
    ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc
    scsi0 : ahci_platform
    scsi1 : ahci_platform
    ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16
    ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16
    m25p80 spi1.0: found m25p05-nonjedec, expected m25p80
    m25p80 spi1.0: m25p05-nonjedec (64 Kbytes)
    Creating 4 MTD partitions on "spi_flash":
    0x000000000000-0x000000040000 : "U-Boot"
    mtd: partition "U-Boot" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
    0x000000010000-0x000000012000 : "U-Boot Env"
    mtd: partition "U-Boot Env" is out of reach -- disabled
    0x000000000000-0x000000280000 : "Kernel"
    mtd: partition "Kernel" extends beyond the end of device "spi_flash" -- size truncated to 0x10000
    0x000000010000-0x000000010000 : "File System"
    mtd: partition "File System" is out of reach -- disabled
    omap2-nand driver initializing
    ONFI flash detected
    ONFI param page 0 valid
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xca (Micron NAND 256MiB 3,3V 16-bit)
    Creating 5 MTD partitions on "omap2-nand.0":
    0x000000000000-0x000000260000 : "U-Boot"
    0x000000260000-0x000000280000 : "U-Boot Env"
    0x000000280000-0x0000006c0000 : "Kernel"
    0x0000006c0000-0x00000cee0000 : "File System"
    0x00000cee0000-0x000010000000 : "Reserved"
    davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    davinci_mdio davinci_mdio.0: detected phy mask fffffff9
    davinci_mdio.0: probed
    davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
    davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver dm9601
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    mice: PS/2 mouse device common for all mice
    omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
    i2c /dev entries driver
    Linux video capture interface: v2.00
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (v1.0.0)
    OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    usbcore: registered new interface driver snd-usb-audio
    asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok
    ALSA device list:
    #0: TI81XX EVM
    TCP cubic registered
    NET: Registered protocol family 17
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    omap_voltage_late_init: Voltage driver support not added
    Power Management for TI81XX.
    smartreflex smartreflex: Driver initialized
    omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
    ata1: SATA link down (SStatus 0 SControl 300)
    ata2: SATA link down (SStatus 0 SControl 300)
    mmc0: new high speed SDHC card at address e624
    mmcblk0: mmc0:e624 SD08G 7.40 GiB
    mmcblk0: p1 p2 p3
    davinci_mdio davinci_mdio.0: resetting idled controller
    net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)
    IP-Config: Complete:
    device=eth0, addr=192.168.0.12, mask=255.255.255.0, gw=192.168.0.1,
    host=192.168.0.12, domain=, nis-domain=(none),
    bootserver=192.168.0.11, rootserver=192.168.0.11, rootpath=
    Root-NFS: nfsroot=/home/sony/targetfs,nolock
    NFS: nfs mount opts='nolock,nolock,addr=192.168.0.11'
    NFS: parsing nfs mount option 'nolock'
    NFS: parsing nfs mount option 'nolock'
    NFS: parsing nfs mount option 'addr=192.168.0.11'
    NFS: MNTPATH: '/home/sony/targetfs'
    NFS: sending MNT request for 192.168.0.11:/home/sony/targetfs
    NFS: failed to create MNT RPC client, status=-113
    NFS: unable to mount server 192.168.0.11, error -113
    VFS: Unable to mount root fs via NFS, trying floppy.
    VFS: Cannot open root device "nfs" or unknown-block(2,0)
    Please append a correct "root=" boot option; here are the available partitions:
    1f00 64 mtdblock0 (driver?)
    1f02 64 mtdblock2 (driver?)
    1f04 2432 mtdblock4 (driver?)
    1f05 128 mtdblock5 (driver?)
    1f06 4352 mtdblock6 (driver?)
    1f07 204928 mtdblock7 (driver?)
    1f08 50304 mtdblock8 (driver?)
    b300 7761920 mmcblk0 driver: mmcblk
    b301 40131 mmcblk0p1 00000000-0000-0000-0000-000000000mmcblk0p1
    b302 883575 mmcblk0p2 00000000-0000-0000-0000-000000000mmcblk0p2
    b303 6835657 mmcblk0p3 00000000-0000-0000-0000-000000000mmcblk0p3
    Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
    Backtrace:
    [<c0049bb8>] (dump_backtrace+0x0/0x110) from [<c039b7d4>] (dump_stack+0x18/0x1c)
    r7:c4bc8000 r6:00000000 r5:c002eb44 r4:c0521710
    [<c039b7bc>] (dump_stack+0x0/0x1c) from [<c039b838>] (panic+0x60/0x17c)
    [<c039b7d8>] (panic+0x0/0x17c) from [<c00092b4>] (mount_block_root+0x1e0/0x220)
    r3:00000000 r2:00000000 r1:c4825f58 r0:c0459cdc
    [<c00090d4>] (mount_block_root+0x0/0x220) from [<c00093a0>] (mount_root+0xac/0xcc)
    [<c00092f4>] (mount_root+0x0/0xcc) from [<c0009530>] (prepare_namespace+0x170/0x1d4)
    r4:c0520f64
    [<c00093c0>] (prepare_namespace+0x0/0x1d4) from [<c00087c4>] (kernel_init+0x114/0x154)
    r5:c00086b0 r4:c0520f00
    [<c00086b0>] (kernel_init+0x0/0x154) from [<c0070c28>] (do_exit+0x0/0x5e4)
    r5:c00086b0 r4:00000000