This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有关SRIO的 SPn_ERR_STAT的问题



使用SRIO让6678和FPGA通信,初始化的时候发现 SPn_ERR_STAT这个寄存器的第二位始终是0,然后我看了这一位的介绍:The input and output ports are initialized and the port is exchanging error-free control symbols with the attached device (read-only).,意思是6678和FPGA之间有个符号没有交换,所以这一位是0吗?