This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335采样偶尔异常问题。



我在做三相并网逆变器的时候,发现偶尔PWM输出一个错误的占空比(大概10几秒出现一次,频率不固定),后来通过测试发现是三相交流电流采样偶尔有问题,即偶尔采到一个突变很厉害的电流点,我的控制方式选择SVPWM控制方式,一个电流采错,会影响我的算法角度都是错的。

具体的测试方式是:

用软件录波的方法,三相电流各设置100个寄存器空间,按3K的频率循环保存AD采样结果寄存器中的值到这个录波空间,并设置一个IO输出口,作为示波器的触发源,示波器采集DSP端口的三相电流的模拟量输入电压(0-3V之间的量),软件可以启动和停止录波,以这个IO口的变位来作为同步标志,这样就能对比我的软件录波和示波器采集的值之间的对应关系。

如下是我软件录波的C相电流结果寄存器中有问题的值,采样电路加了1.5V偏置,即0到3V范围代表电流从-500A到+500A的范围,出现了一个1072的采样值,代表电流值大概是-480A左右,和上下文关系明显不对,以及对比了示波器上的波形,其他点是对的上的,但是这个点在示波器上是没有反应的。我们的软件录波是3K的频率,示波器的带宽是20M,照理如果软件采到一个异常值,示波器上面的模拟量输入值应该有对应关系。所以,想问大家的是,有谁遇到过这个比较怪异的现象不?我应该从哪方面着手,接着测试呢?谢谢!

38464
38240
38128
1072
39056