This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XGBE 10GE



66AK2E05XABD25定制板

使用ti-processor-sdk-linux-rt-k2e-evm-05.02.00.10-Linux-x86-Install.bin开发包

已在keystone-k2e-netcp.dtsi配置xgbe接口,配置如下:

xgbe_subsys: subsys@2f00000 {
 status  = "disabled";
 compatible = "syscon";
 reg  = <0x02f00000 0x100>;
};
xgbe_pcsr: pcsr@2f00600 {
 status  = "disabled";
 compatible = "syscon";
 reg  = <0x02f00600 0x100>;
};
xgbe_serdes: phy@231e000 {
 #phy-cells  = <0>;
 compatible  = "ti,keystone-serdes-xgbe";
 reg   = <0x0231e000 0x2000>;
 status   = "disabled";
 link-rate-kbps  = <10312500>;
 num-lanes  = <2>;
 syscon-peripheral = <&xgbe_subsys>;
 syscon-link  = <&xgbe_pcsr>;
 #address-cells = <1>;
 #size-cells = <0>;
 xserdes_lane0: lane@0 {
  #phy-cells = <0>;
  reg  = <0>;
  status  = "ok";
  control-rate = <0>;
  rx-start = <7 5>;
  rx-force = <1 1>;
  tx-coeff = <2 0 0 12 4>;
 };
 xserdes_lane1: lane@1 {
  #phy-cells = <0>;
  reg  = <1>;
  status  = "ok";
  control-rate = <0>;
  rx-start = <7 5>;
  rx-force = <1 1>;
  tx-coeff = <2 0 0 12 4>;
 };
};
netcpx: netcp@2f00000 {
 status  = "disabled";
 compatible = "ti,netcp-1.0";
 #address-cells = <1>;
 #size-cells = <1>;
 ranges;
 clocks  = <&clkxge>, <&chipclk12>;
 clock-names = "xge_clk", "cpts";
 dma-coherent;
 ti,navigator-dmas = <&dma_xgbe 0>,
   <&dma_xgbe 8>,
   <&dma_xgbe 0>;
 ti,navigator-dma-names = "xnetrx0", "xnetrx1", "xnettx";
 netcp-devices {
  #address-cells = <1>;
  #size-cells = <1>;
  ranges;
  xgbe@2f00000 {
   label = "netcp-xgbe";
   compatible = "ti,netcp-xgbe";
   syscon-subsys = <&xgbe_subsys>;
   syscon-pcsr = <&xgbe_pcsr>;
   reg = <0x02f00100 0x200>, <0x02f01000 0xb00>;
   tx-queue = <692>;
   tx-channel = "xnettx";
   interfaces {
    xgbe0: interface-0 {
     phys  = <&xserdes_lane0>;
     slave-port = <0>;
     link-interface = <11>;
    };
    xgbe1: interface-1 {
     phys  = <&xserdes_lane1>;
     slave-port = <1>;
     link-interface = <11>;
    };
   };
  };
 };
 netcp-interfaces {
  interface-0 {
   rx-channel = "xnetrx0";
   rx-pool = <2048 12>;
   tx-pool = <1024 12>;
   rx-queue-depth = <1024 1024 0 0>;
   rx-buffer-size = <1536 4096 0 0>;
   rx-queue = <532>;
   tx-completion-queue = <534>;
   efuse-mac = <0>;
   netcp-xgbe = <&xgbe0>;
  };
  interface-1 {
   rx-channel = "xnetrx1";
   rx-pool = <2048 12>;
   tx-pool = <1024 12>;
   rx-queue-depth = <1024 1024 0 0>;
   rx-buffer-size = <1536 4096 0 0>;
   rx-queue = <533>;
   tx-completion-queue = <535>;
   efuse-mac = <0>;
   netcp-xgbe = <&xgbe1>;
  };
 };
};

XFITX/XFIRX与SFP+ 1888247-2&2007194-1直连

已将TX_DISABLE拉低使能传输,RATE_SELECT拉高

使用LC-LC多模光纤与INTEL(R) ETH CONVERGED NTWK ADPTR X520-SR2连接

故障现象:

INTEL(R)万兆以太网卡一直重复 连接-断开-连接-断开

请问是对xgbe接口配置有问题还是硬件设计有问题,该如何修改,谢谢