This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728 dsp 核gpio 中断问题

Other Parts Discussed in Thread: AM5728

AM5728   DSP  (基于YSYBIOS )

参照GPIO_LedBlink_evmAM572x_c66xExampleProject_with_ipc 

用GPIO3_22 (KEY5)作为外部触发中断

#define GPIO_USER0_LED_PIN_NUM    (0x08)
#define GPIO_USER0_LED_PORT_NUM   (0x07)
#define GPIO_USER1_LED_PIN_NUM    (0x14)
#define GPIO_USER1_LED_PORT_NUM   (0x03)

#define GPIO_INT_KEY5_PORT_NUM     (0x03)
#define GPIO_INT_KEY5_PIN_NUM     (0x16)

/* GPIO Driver board specific pin configuration structure */
GPIO_PinConfig gpioPinConfigs[] = {
    /* Input pin with interrupt enabled : AM57X_IDK_GRN_LED */
    //GPIO_DEVICE_CONFIG(GPIO_USER0_LED_PORT_NUM, GPIO_USER0_LED_PIN_NUM) |
    //GPIO_CFG_IN_INT_RISING | GPIO_CFG_INPUT,

   // 下降沿中断 按键5  *******////////
   GPIO_DEVICE_CONFIG(GPIO_INT_KEY5_PORT_NUM, GPIO_INT_KEY5_PIN_NUM) |
   GPIO_CFG_IN_INT_FALLING | GPIO_CFG_INPUT
    /* Output pin : AM57X_IDK_YEL_LED */
    GPIO_DEVICE_CONFIG(GPIO_USER1_LED_PORT_NUM, GPIO_USER1_LED_PIN_NUM) |
    GPIO_CFG_OUTPUT ,
};
/* GPIO Driver call back functions */
GPIO_CallbackFxn gpioCallbackFunctions[] = {
    NULL,
    NULL
};
/* GPIO Driver configuration structure */
GPIO_v1_Config GPIO_v1_config = {
    gpioPinConfigs,
    gpioCallbackFunctions,
    sizeof(gpioPinConfigs) / sizeof(GPIO_PinConfig),
    sizeof(gpioCallbackFunctions) / sizeof(GPIO_CallbackFxn),
    0x20,
    };

在主程序中初始化板子、GPIO 、设置回调函数,使能中断。 但是就是无法进入中断, 去掉中断配置项测试,在KEY5按下时可以读到引脚的点评变化。请问是别的地方还需要配置什么么?