This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用仿真器连接AM5728提示501或233错误

Other Parts Discussed in Thread: AM5728

你好:

在使用SEED xds560v2 USB emulator通过JTAG连接一块AM5728开发板DSP时,ccs(版本8.3.0)中Test Connection报错:
[Start: SEED XDS560V2 USB Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -F inform,logfile=yes -S pathlength -S integrity

[Result]

-----[Print the board config pathname(s)]------------------------------------

C:\Users\admin\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'seed560v2u.out'.
Loaded FPGA Image: E:\ti\ccsv8\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'Nov 20 2018'.
The library build time was '23:11:38'.
The library package version is '8.0.903.2'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '6' (0x00000006).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the Nano-TBC VHDL.
The link is a 560-class second-generation-560 cable.
The software is configured for Nano-TBC VHDL features.
The controller will be software reset via its registers.
The controller has a logic ONE on its EMU[0] input pin.
The controller has a logic ONE on its EMU[1] input pin.
The controller will use falling-edge timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '2' (0x0002).
The utility logic has not previously detected a power-loss.
The utility logic is not currently detecting a power-loss.
Loaded FPGA Image: E:\ti\ccsv8\ccs_base\common\uscif\dtc_top.jbc

An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-501' (0xfffffe0b).
The title is 'SC_ERR_TEST_MEASURE'.

The explanation is:
The built-in scan-path length measurement failed.
The built-in scan-path reliability tests cannot be
performed without knowledge of the scan-path length.
Try specifying the scan-path lengths in the command-line
options or board configuration file of this utility or debugger.

另外改变改变JTAG TCLK频率也没有效果,有时候也会报下面错误:

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

请帮忙看下什么原因。非常感谢。