am335x-bone-common.dtsi中添加
spi1_pins_default: spi1_pins_default { pinctrl-single,pins = < AM33XX_IOPAD(0x990, PIN_INPUT_PULLUP | MUX_MODE3) /* (A13) mcasp0_aclkx.spi1_sclk */ AM33XX_IOPAD(0x994, PIN_INPUT_PULLUP | MUX_MODE3) /* (B13) mcasp0_fsx.spi1_d0 */ AM33XX_IOPAD(0x998, PIN_OUTPUT_PULLUP | MUX_MODE3) /* (D12) mcasp0_axr0.spi1_d1 */ AM33XX_IOPAD(0x99c, PIN_OUTPUT_PULLUP | MUX_MODE3) /* (C12) mcasp0_ahclkr.spi1_cs0 */ >; };
&spi1 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spi1_pins_default>;
channel@0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "spidev";
reg = <0>;
spi-max-frequency = <16000000>;
spi-cpha;
};
};
编译好后,进入系统,dmesg显示spi1的pinctrl占用了macsp的管脚,注册了spidev1.0设备,短接D0和D1
./spifdv_test -D /dev/spidev1.0
该命令只打印出spi1的mode,发送模式和工作频率,并没有发送数据的过程